sl_btmesh_evt_prov_initialization_failed#

Provisioner has not been initialized successfully and is not operational.

It is not possible to use the device as a Provisioner. See the result code for details.

Modules#

sl_btmesh_evt_prov_initialization_failed_s

Macros#

#define

Identifier of the initialization_failed event.

Typedef Documentation#

sl_btmesh_evt_prov_initialization_failed_t#

typedef struct sl_btmesh_evt_prov_initialization_failed_s sl_btmesh_evt_prov_initialization_failed_t

Definition at line 2642 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_prov_initialization_failed_id#

#define sl_btmesh_evt_prov_initialization_failed_id
Value:
0x1b1500a8

Identifier of the initialization_failed event.


Definition at line 2632 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h