OOB Capabilities#

OOB capability bitmask constants

Macro Definition Documentation#

SL_BTMESH_PROV_OOB_OTHER#

#define SL_BTMESH_PROV_OOB_OTHER
Value:
0x1

Uncategorized


Definition at line 2150 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_URI#

#define SL_BTMESH_PROV_OOB_URI
Value:
0x2

URI or other electronic


Definition at line 2153 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_2D_MR_CODE#

#define SL_BTMESH_PROV_OOB_2D_MR_CODE
Value:
0x4

2D machine-readable code


Definition at line 2156 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_BAR_CODE#

#define SL_BTMESH_PROV_OOB_BAR_CODE
Value:
0x8

Barcode


Definition at line 2159 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_NFC#

#define SL_BTMESH_PROV_OOB_NFC
Value:
0x10

NFC


Definition at line 2162 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_NUMBER#

#define SL_BTMESH_PROV_OOB_NUMBER
Value:
0x20

Number


Definition at line 2165 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_STRING#

#define SL_BTMESH_PROV_OOB_STRING
Value:
0x40

String


Definition at line 2168 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_RFU_7#

#define SL_BTMESH_PROV_OOB_RFU_7
Value:
0x80

Reserved


Definition at line 2171 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_RFU_8#

#define SL_BTMESH_PROV_OOB_RFU_8
Value:
0x100

Reserved


Definition at line 2174 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_RFU_9#

#define SL_BTMESH_PROV_OOB_RFU_9
Value:
0x200

Reserved


Definition at line 2177 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_RFU_A#

#define SL_BTMESH_PROV_OOB_RFU_A
Value:
0x400

Reserved


Definition at line 2180 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_LOC_ON_BOX#

#define SL_BTMESH_PROV_OOB_LOC_ON_BOX
Value:
0x800

On the box


Definition at line 2183 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_LOC_IN_BOX#

#define SL_BTMESH_PROV_OOB_LOC_IN_BOX
Value:
0x1000

Inside the box


Definition at line 2186 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_LOC_PAPER#

#define SL_BTMESH_PROV_OOB_LOC_PAPER
Value:
0x2000

On a piece of paper


Definition at line 2189 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_LOC_MANUAL#

#define SL_BTMESH_PROV_OOB_LOC_MANUAL
Value:
0x4000

In the device manual


Definition at line 2192 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_LOC_DEVICE#

#define SL_BTMESH_PROV_OOB_LOC_DEVICE
Value:
0x8000

On the device


Definition at line 2195 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

SL_BTMESH_PROV_OOB_RFU_MASK#

#define SL_BTMESH_PROV_OOB_RFU_MASK
Value:
0x780

Mask of reserved bits


Definition at line 2198 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h