sl_btmesh_evt_sar_config_client_sar_receiver_status#
SAR Reveiver state parameters, reply for a sl_btmesh_sar_config_client_get_sar_receiver or sl_btmesh_sar_config_client_set_sar_receiver command.
Modules#
sl_btmesh_evt_sar_config_client_sar_receiver_status_s
Typedefs#
Macros#
#define
Identifier of the sar_receiver_status event.
Typedef Documentation#
sl_btmesh_evt_sar_config_client_sar_receiver_status_t#
typedef struct sl_btmesh_evt_sar_config_client_sar_receiver_status_s sl_btmesh_evt_sar_config_client_sar_receiver_status_t
Definition at line
20611
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_sar_config_client_sar_receiver_status_id#
#define sl_btmesh_evt_sar_config_client_sar_receiver_status_idValue:
0x026200a8
Identifier of the sar_receiver_status event.
Definition at line
20550
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h