sl_btmesh_evt_sar_config_client_sar_transmitter_status#

SAR Transmitter state parameters, reply for a sl_btmesh_sar_config_client_get_sar_transmitter or sl_btmesh_sar_config_client_set_sar_transmitter command.

Modules#

sl_btmesh_evt_sar_config_client_sar_transmitter_status_s

Macros#

#define

Identifier of the sar_transmitter_status event.

Typedef Documentation#

sl_btmesh_evt_sar_config_client_sar_transmitter_status_t#

typedef struct sl_btmesh_evt_sar_config_client_sar_transmitter_status_s sl_btmesh_evt_sar_config_client_sar_transmitter_status_t

Definition at line 20537 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_sar_config_client_sar_transmitter_status_id#

#define sl_btmesh_evt_sar_config_client_sar_transmitter_status_id
Value:
0x016200a8

Identifier of the sar_transmitter_status event.


Definition at line 20407 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h