Data structure of the status event.

Public Attributes#

uint16_t
uint16_t
uint16_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_scheduler_client_status_s::client_address

Destination client model address


elem_index#

uint16_t sl_btmesh_evt_scheduler_client_status_s::elem_index

Client model element index


server_address#

uint16_t sl_btmesh_evt_scheduler_client_status_s::server_address

Source server model address


appkey_index#

uint16_t sl_btmesh_evt_scheduler_client_status_s::appkey_index

The application key index to use.


scheduler#

uint16_t sl_btmesh_evt_scheduler_client_status_s::scheduler

Bit field indicating defined Actions in the Schedule Register