sl_btmesh_evt_sensor_client_status#
Indicate an incoming Sensor Status event as a published data state from the sensor server or as a reply to the sl_btmesh_sensor_client_get command.
Modules#
sl_btmesh_evt_sensor_client_status_s
Typedefs#
Macros#
#define
sl_btmesh_evt_sensor_client_status_id 0x044900a8
Identifier of the status event.
Typedef Documentation#
sl_btmesh_evt_sensor_client_status_t#
typedef struct sl_btmesh_evt_sensor_client_status_s sl_btmesh_evt_sensor_client_status_t
Definition at line
12531
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_sensor_client_status_id#
#define sl_btmesh_evt_sensor_client_status_idValue:
0x044900a8
Identifier of the status event.
Definition at line
12502
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h