Data structure of the network_pdu_status event.
Public Attribute Documentation#
server#
uint16_t sl_btmesh_evt_silabs_config_client_network_pdu_status_s::server
Server address.
Definition at line
3878
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
status#
uint8_t sl_btmesh_evt_silabs_config_client_network_pdu_status_s::status
Enum sl_btmesh_silabs_config_client_status_t. Status code from the Server.
Definition at line
3879
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
pdu_max_size#
uint16_t sl_btmesh_evt_silabs_config_client_network_pdu_status_s::pdu_max_size
Network PDU max size
Definition at line
3881
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h