Data structure of the tx_status event.
Public Attribute Documentation#
status#
uint8_t sl_btmesh_evt_silabs_config_client_tx_status_s::status
Enum sl_btmesh_silabs_config_client_status_t. Status code from the Server.
tx_phy#
uint8_t sl_btmesh_evt_silabs_config_client_tx_status_s::tx_phy
TX PHY for long packets (packets that would be segmented).
1: LE 1M PHY
2: LE 2M PHY
tx_options_bitmap#
uint32_t sl_btmesh_evt_silabs_config_client_tx_status_s::tx_options_bitmap
TX options. NOTE: Currently not used: reserved for future use.