sl_btmesh_evt_silabs_config_server_tx_changed#

TX PHY configuration value has changed.

New values included in the parameters.

Modules#

sl_btmesh_evt_silabs_config_server_tx_changed_s

Macros#

#define

Identifier of the tx_changed event.

Typedef Documentation#

sl_btmesh_evt_silabs_config_server_tx_changed_t#

typedef struct sl_btmesh_evt_silabs_config_server_tx_changed_s sl_btmesh_evt_silabs_config_server_tx_changed_t

Definition at line 22152 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_silabs_config_server_tx_changed_id#

#define sl_btmesh_evt_silabs_config_server_tx_changed_id
Value:
0x006b00a8

Identifier of the tx_changed event.


Definition at line 22137 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h