Data structure of the tx_changed event.

Public Attributes#

uint8_t
uint32_t

Public Attribute Documentation#

phy#

uint8_t sl_btmesh_evt_silabs_config_server_tx_changed_s::phy

TX PHY for long packets (packets that would be segmented).

  • 1: LE 1M PHY

  • 2: LE 2M PHY


Definition at line 22144 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

options#

uint32_t sl_btmesh_evt_silabs_config_server_tx_changed_s::options

TX options. NOTE: Currently not used: reserved for future use.


Definition at line 22148 of file /mnt/raid/workspaces/ws.Z1571VLo9/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h