sl_btmesh_evt_time_client_time_zone_status#

Time Zone Status event, response to sl_btmesh_time_client_set_time_zone or sl_btmesh_time_client_get_time_zone command or unsolicited message.

Modules#

sl_btmesh_evt_time_client_time_zone_status_s

Macros#

#define

Identifier of the time_zone_status event.

Typedef Documentation#

sl_btmesh_evt_time_client_time_zone_status_t#

typedef struct sl_btmesh_evt_time_client_time_zone_status_s sl_btmesh_evt_time_client_time_zone_status_t

Definition at line 16606 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_time_client_time_zone_status_id#

#define sl_btmesh_evt_time_client_time_zone_status_id
Value:
0x015300a8

Identifier of the time_zone_status event.


Definition at line 16587 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h