sl_btmesh_evt_time_client_tai_utc_delta_status#

TAI-UTC Delta Status event, response to sl_btmesh_time_client_set_tai_utc_delta or sl_btmesh_time_client_get_tai_utc_delta command or unsolicited message.

Modules#

sl_btmesh_evt_time_client_tai_utc_delta_status_s

Macros#

#define

Identifier of the tai_utc_delta_status event.

Typedef Documentation#

sl_btmesh_evt_time_client_tai_utc_delta_status_t#

typedef struct sl_btmesh_evt_time_client_tai_utc_delta_status_s sl_btmesh_evt_time_client_tai_utc_delta_status_t

Definition at line 16638 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_time_client_tai_utc_delta_status_id#

#define sl_btmesh_evt_time_client_tai_utc_delta_status_id
Value:
0x025300a8

Identifier of the tai_utc_delta_status event.


Definition at line 16619 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h