Data structure of the tai_utc_delta_status event.

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::client_address

Client address


elem_index#

uint16_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::elem_index

Client model element index


server_address#

uint16_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::server_address

Unicast address of the server


appkey_index#

uint16_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::appkey_index

App key index.


tai_utc_delta_current#

int32_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::tai_utc_delta_current

Current difference between TAI and UTC. Range is -255 to 32512.


tai_utc_delta_new#

int32_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::tai_utc_delta_new

Upcoming difference between TAI and UTC in seconds. Range is -255 to 32512.


tai_of_delta_change#

uint64_t sl_btmesh_evt_time_client_tai_utc_delta_status_s::tai_of_delta_change

TAI seconds time of the upcoming TAI-UTC delta change