Data structure of the heartbeat_pub_status event.

Public Attributes#

uint16_t
uint32_t
uint16_t
uint8_t
uint8_t
uint8_t
uint16_t

Public Attribute Documentation#

result#

uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::result

SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8573 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

handle#

uint32_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::handle

Request handle


Definition at line 8575 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

destination_address#

uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::destination_address

Heartbeat publication destination address.


Definition at line 8576 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

netkey_index#

uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::netkey_index

Index of the network key used to encrypt heartbeat messages


Definition at line 8577 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

count_log#

uint8_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::count_log

Heartbeat publication count logarithm-of-2 setting


Definition at line 8579 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

period_log#

uint8_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::period_log

Heartbeat publication period logarithm-of-2 setting


Definition at line 8581 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

ttl#

uint8_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::ttl

Time-to-live value for heartbeat messages


Definition at line 8583 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

features#

uint16_t sl_btmesh_evt_config_client_heartbeat_pub_status_s::features

Heartbeat trigger setting


Definition at line 8584 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h