Data structure of the capabilities_status event.

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::elem_index

Client model element index


Definition at line 18467 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::server_address

Unicast address of the server


Definition at line 18468 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

max_nodes_list_size#

uint16_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::max_nodes_list_size

Maximum number of entries the node list can contain


Definition at line 18469 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

max_fw_list_size#

uint16_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::max_fw_list_size

Maximum number of entries the Firmware List can contain


Definition at line 18471 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

max_fw_size#

uint32_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::max_fw_size

Maximum size of a single firmware image


Definition at line 18473 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

max_upload_space#

uint32_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::max_upload_space

Maximum number of bytes for firmware images


Definition at line 18475 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

remaining_upload_space#

uint32_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::remaining_upload_space

Remaining number of bytes for firmware images


Definition at line 18477 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

oob_supported#

uint8_t sl_btmesh_evt_fw_dist_client_capabilities_status_s::oob_supported

Enum sl_btmesh_fw_dist_client_dist_oob_t. OOB firmware retrieval (using the Update URI received from an Update Server) supported


Definition at line 18479 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

uri_scheme_names#

uint8array sl_btmesh_evt_fw_dist_client_capabilities_status_s::uri_scheme_names

Supported URI scheme names. Empty if OOB is not supported.


Definition at line 18484 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h