Data structure of the receivers_list_end event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::elem_index
Client model element index
Definition at line
18442
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::server_address
Unicast address of the server
Definition at line
18443
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
start_index#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::start_index
Starting index
Definition at line
18444
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
num_reported#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::num_reported
Number of entries reported
Definition at line
18445
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
nodes_list_size#
uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_end_s::nodes_list_size
Number of entries currently in the node list
Definition at line
18446
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h