Data structure of the receivers_list event.

Public Attributes#

uint16_t
uint16_t
uint16_t
uint8_t
uint8_t
uint8_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::elem_index

Client model element index


Definition at line 18407 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::server_address

Unicast address of the server


Definition at line 18408 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

index#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::index

Index of the entry reported


Definition at line 18409 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

nodes_list_size#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::nodes_list_size

Number of entries currently in the node list


Definition at line 18410 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

address#

uint16_t sl_btmesh_evt_fw_dist_client_receivers_list_s::address

Address of the Update Server


Definition at line 18411 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

phase#

uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::phase

Enum sl_btmesh_fw_dist_server_dist_node_phase_t. Phase of the Update Server


Definition at line 18412 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

update_status#

uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::update_status

Last Update Status message received from the Update Server


Definition at line 18415 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

transfer_status#

uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::transfer_status

Last Transfer Status message received from the BLOB Transfer Server


Definition at line 18417 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

progress#

uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::progress

0-100, percentage of BLOB Transfer octets delivered and confirmed


Definition at line 18419 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

fw_index#

uint8_t sl_btmesh_evt_fw_dist_client_receivers_list_s::fw_index

Index of the firmware being updated


Definition at line 18421 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h