Data structure of the dist_start_req event.
Public Attribute Documentation#
elem_index#
uint16_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::elem_index
Server model element index
Definition at line
17405
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
client_address#
uint16_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::client_address
Address of the Distribution Client
Definition at line
17406
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
group_address#
uint16_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::group_address
Group address of the distribution
Definition at line
17407
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
virtual_address#
uuid_128 sl_btmesh_evt_fw_dist_server_dist_start_req_s::virtual_address
If the group address is a VA hash, this contains the full virtual address label UUID of the distribution. Otherwise, the value of this field should be ignored.
Definition at line
17408
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
ttl#
uint8_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::ttl
Distribution TTL
Definition at line
17412
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
apply_immediately#
uint8_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::apply_immediately
Enum sl_btmesh_fw_dist_server_dfu_policy_t. 1 if the Update Policy is Verify and Apply, otherwise 0.
Definition at line
17413
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
fw_list_index#
uint16_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::fw_list_index
Index of the firmware in the Distributor's FW List
Definition at line
17417
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
timeout_base#
uint16_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::timeout_base
Timeout base
Definition at line
17419
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
transfer_mode#
uint8_t sl_btmesh_evt_fw_dist_server_dist_start_req_s::transfer_mode
Transfer Mode to use in the distribution
Definition at line
17420
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h