Data structure of the nodes_deleted event.

Public Attributes#

uint16_t

Public Attribute Documentation#

elem_index#

uint16_t sl_btmesh_evt_fw_dist_server_nodes_deleted_s::elem_index

Server model element index


Definition at line 17383 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

client_address#

uint16_t sl_btmesh_evt_fw_dist_server_nodes_deleted_s::client_address

Address of the Distribution Client


Definition at line 17384 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h