Data structure of the server_status_attention event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_health_client_server_status_attention_s::client_address
Destination address the message was sent to
Definition at line
4688
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_health_client_server_status_attention_s::elem_index
Client model element index. Identifies the client model which received the status message.
Definition at line
4689
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_health_client_server_status_attention_s::server_address
Address of the Server model which sent the message
Definition at line
4691
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
result#
uint16_t sl_btmesh_evt_health_client_server_status_attention_s::result
Response status. If an error occurs (e.g., request timeout), ignore the parameters other than element index, client address, and server address.
Definition at line
4693
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
attention_sec#
uint8_t sl_btmesh_evt_health_client_server_status_attention_s::attention_sec
Current attention timer value in seconds
Definition at line
4697
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h