Data structure of the server_status_period event.

Public Attributes#

uint16_t
uint16_t
uint8_t

Public Attribute Documentation#

client_address#

uint16_t sl_btmesh_evt_health_client_server_status_period_s::client_address

Destination address the message was sent to


Definition at line 4651 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

elem_index#

uint16_t sl_btmesh_evt_health_client_server_status_period_s::elem_index

Client model element index. Identifies the client model, which received the status message.


Definition at line 4652 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

server_address#

uint16_t sl_btmesh_evt_health_client_server_status_period_s::server_address

Address of the Server model which sent the message


Definition at line 4654 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

result#

uint16_t sl_btmesh_evt_health_client_server_status_period_s::result

Response status. If an error occurs (e.g., request timeout), ignore the parameters other than element index, client address, and server address.


Definition at line 4656 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

period#

uint8_t sl_btmesh_evt_health_client_server_status_period_s::period

Health period divisor value


Definition at line 4660 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h