Data structure of the mode_status event.
Public Attribute Documentation#
destination_address#
uint16_t sl_btmesh_evt_lc_client_mode_status_s::destination_address
Address of the client or the group address to which it was published.
Definition at line
13564
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_lc_client_mode_status_s::elem_index
Index of the element for which received the status.
Definition at line
13566
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_lc_client_mode_status_s::server_address
Device which sent the status.
Definition at line
13568
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_lc_client_mode_status_s::appkey_index
Appkey used by server_address.
Definition at line
13569
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
mode_status_value#
uint8_t sl_btmesh_evt_lc_client_mode_status_s::mode_status_value
Value reported by server.
Definition at line
13570
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h