Data structure of the data_header event.

Public Attributes#

uint32_t
uint16_t
uint16_t

Public Attribute Documentation#

handle#

uint32_t sl_btmesh_evt_lcd_client_data_header_s::handle

Request handle


Definition at line 21738 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

page_number#

uint8_t sl_btmesh_evt_lcd_client_data_header_s::page_number

Page number of the Composition Data


Definition at line 21739 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

offset#

uint16_t sl_btmesh_evt_lcd_client_data_header_s::offset

Offset within the page


Definition at line 21740 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

total_size#

uint16_t sl_btmesh_evt_lcd_client_data_header_s::total_size

Total size of the page


Definition at line 21741 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h