Data structure of the descriptor_status event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_sensor_client_descriptor_status_s::client_address
Destination client model address
Definition at line
12435
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_sensor_client_descriptor_status_s::elem_index
Client model element index
Definition at line
12436
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_sensor_client_descriptor_status_s::server_address
Source server model address
Definition at line
12437
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_sensor_client_descriptor_status_s::appkey_index
The application key index to use.
Definition at line
12438
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
flags#
uint8_t sl_btmesh_evt_sensor_client_descriptor_status_s::flags
No flags defined currently
Definition at line
12439
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
descriptors#
uint8array sl_btmesh_evt_sensor_client_descriptor_status_s::descriptors
One or more Sensor Descriptor states (N times 8 bytes) As a reply to a Get message referencing a sensor that does not exist, the array contains only the requested Property ID. Format of the Descriptor state is as follows:
Property ID, 16 bits
Sensor Positive Tolerance, 12 bits
Sensor Negative Tolerance, 12 bits
Sensor Sampling Function, 8 bits
Sensor Measurement Period, 8 bits
Sensor Update Interval, 8 bits {/ul>
Definition at line
12440
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h