Data structure of the series_status event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_sensor_client_series_status_s::client_address
Destination client model address
12674
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_sensor_client_series_status_s::elem_index
Client model element index
12675
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_sensor_client_series_status_s::server_address
Source server model address
12676
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_sensor_client_series_status_s::appkey_index
The application key index to use
12677
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
flags#
uint8_t sl_btmesh_evt_sensor_client_series_status_s::flags
No flags defined currently
12678
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
property_id#
uint16_t sl_btmesh_evt_sensor_client_series_status_s::property_id
Property ID for the sensor. Range: 0x0001 - 0x0ffff for a specific device property, the value 0x0000 is prohibited.
12679
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
sensor_data#
uint8array sl_btmesh_evt_sensor_client_series_status_s::sensor_data
Byte array containing the serialized sequence of Sensor Serier Column states in the following format:
1st Sensor Raw Value X, variable length raw value representing the left corner of a column
1st Sensor Column Width, variable length raw value representing the width of the column
1st Sensor Raw Value Y, variable length raw value representing the height of the column
...
Nth Sensor Raw Value X, variable length raw value representing the left corner of a column
Nth Sensor Column Width, variable length raw value representing the width of the column
Nth Sensor Raw Value Y, variable length raw value representing the height of the column
If a Property ID or column requested does not exist at the server element, the reply Series Status message contains only the given Property ID.
12682
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h