Data structure of the time_role_status event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_time_client_time_role_status_s::client_address
Client address
Definition at line
16736
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_time_client_time_role_status_s::elem_index
Client model element index
Definition at line
16737
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_time_client_time_role_status_s::server_address
Unicast address of the server
Definition at line
16738
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_time_client_time_role_status_s::appkey_index
App key index.
Definition at line
16739
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
time_role#
uint8_t sl_btmesh_evt_time_client_time_role_status_s::time_role
The Time Role for the element
Definition at line
16740
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h