Data structure of the time_zone_status event.
Public Attribute Documentation#
client_address#
uint16_t sl_btmesh_evt_time_client_time_zone_status_s::client_address
Client address
Definition at line
16672
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
elem_index#
uint16_t sl_btmesh_evt_time_client_time_zone_status_s::elem_index
Client model element index
Definition at line
16673
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
server_address#
uint16_t sl_btmesh_evt_time_client_time_zone_status_s::server_address
Unicast address of the server
Definition at line
16674
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
appkey_index#
uint16_t sl_btmesh_evt_time_client_time_zone_status_s::appkey_index
App key index.
Definition at line
16675
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
time_zone_offset_current#
int16_t sl_btmesh_evt_time_client_time_zone_status_s::time_zone_offset_current
Current local time zone offset. Range is -64 to 191, representing -16 to 47.75 hours.
Definition at line
16676
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
time_zone_offset_new#
int16_t sl_btmesh_evt_time_client_time_zone_status_s::time_zone_offset_new
Upcoming local time zone offset
Definition at line
16679
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
tai_of_zone_change#
uint64_t sl_btmesh_evt_time_client_time_zone_status_s::tai_of_zone_change
TAI seconds time of the upcoming Time Zone offset change
Definition at line
16680
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h