sl_btmesh_evt_config_client_appkey_status#
This event is created when a response for an sl_btmesh_config_client_add_appkey or a sl_btmesh_config_client_remove_appkey request is received or the request times out.
Modules#
sl_btmesh_evt_config_client_appkey_status_s
Typedefs#
Macros#
#define
sl_btmesh_evt_config_client_appkey_status_id 0x042700a8
Identifier of the appkey_status event.
Typedef Documentation#
sl_btmesh_evt_config_client_appkey_status_t#
typedef struct sl_btmesh_evt_config_client_appkey_status_s sl_btmesh_evt_config_client_appkey_status_t
Definition at line
8309
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_config_client_appkey_status_id#
#define sl_btmesh_evt_config_client_appkey_status_idValue:
0x042700a8
Identifier of the appkey_status event.
Definition at line
8298
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h