sl_btmesh_evt_config_client_model_sub_status#

Status event for sl_btmesh_config_client_add_model_sub : add subscription address, sl_btmesh_config_client_add_model_sub_va : add subscription virtual address, sl_btmesh_config_client_remove_model_sub : remove subscription address, sl_btmesh_config_client_remove_model_sub_va : remove subscription virtual address, sl_btmesh_config_client_set_model_sub : set subscription address, sl_btmesh_config_client_set_model_sub_va : set subscription virtual address, and sl_btmesh_config_client_clear_model_sub : clear subscription address list commands.

Modules#

sl_btmesh_evt_config_client_model_sub_status_s

Macros#

#define

Identifier of the model_sub_status event.

Typedef Documentation#

sl_btmesh_evt_config_client_model_sub_status_t#

typedef struct sl_btmesh_evt_config_client_model_sub_status_s sl_btmesh_evt_config_client_model_sub_status_t

Definition at line 8503 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_config_client_model_sub_status_id#

#define sl_btmesh_evt_config_client_model_sub_status_id
Value:
0x0b2700a8

Identifier of the model_sub_status event.


Definition at line 8492 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h