sl_btmesh_evt_config_client_bindings_list#

This event contains a list of key indices for the application keys which are bound to a model.

The list is requested using the sl_btmesh_config_client_list_bindings command. More than one such event may be generated; the list contents are terminated by a sl_btmesh_evt_config_client_bindings_list_end event.

Modules#

sl_btmesh_evt_config_client_bindings_list_s

Macros#

#define

Identifier of the bindings_list event.

Typedef Documentation#

sl_btmesh_evt_config_client_bindings_list_t#

typedef struct sl_btmesh_evt_config_client_bindings_list_s sl_btmesh_evt_config_client_bindings_list_t

Definition at line 8411 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_config_client_bindings_list_id#

#define sl_btmesh_evt_config_client_bindings_list_id
Value:
0x082700a8

Identifier of the bindings_list event.


Definition at line 8399 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h