sl_btmesh_evt_config_client_request_modified#
Pending request parameters have been updated.
The application may call sl_btmesh_config_client_get_request_status to retrieve the current status of the request. This event is generated when the timeout of a request is extended because the request is acknowledged by a Friend node on behalf of the LPN, which is the destination of the request.
Modules#
sl_btmesh_evt_config_client_request_modified_s
Typedefs#
Macros#
#define
Identifier of the request_modified event.
Typedef Documentation#
sl_btmesh_evt_config_client_request_modified_t#
typedef struct sl_btmesh_evt_config_client_request_modified_s sl_btmesh_evt_config_client_request_modified_t
Definition at line
8209
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_config_client_request_modified_id#
#define sl_btmesh_evt_config_client_request_modified_idValue:
0x002700a8
Identifier of the request_modified event.
Definition at line
8199
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h