sl_btmesh_evt_mbt_client_server_block_status#

The MBT Server's current block status.

This event contains the current block status received from a MBT Server. The status is received as a response to sl_btmesh_mbt_client_start_block or sl_btmesh_mbt_client_query_block_status commands.

Modules#

sl_btmesh_evt_mbt_client_server_block_status_s

Macros#

#define

Identifier of the server_block_status event.

Typedef Documentation#

sl_btmesh_evt_mbt_client_server_block_status_t#

typedef struct sl_btmesh_evt_mbt_client_server_block_status_s sl_btmesh_evt_mbt_client_server_block_status_t

Definition at line 10482 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_mbt_client_server_block_status_id#

#define sl_btmesh_evt_mbt_client_server_block_status_id
Value:
0x032800a8

Identifier of the server_block_status event.


Definition at line 10467 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h