sl_btmesh_evt_mbt_client_server_failed#

A server failed and was removed from the transfer.

This event indicates that a server timed out or reported an irrecoverable error. A failed server is removed from the transfer.

Modules#

sl_btmesh_evt_mbt_client_server_failed_s

Macros#

#define

Identifier of the server_failed event.

Typedef Documentation#

sl_btmesh_evt_mbt_client_server_failed_t#

typedef struct sl_btmesh_evt_mbt_client_server_failed_s sl_btmesh_evt_mbt_client_server_failed_t

Definition at line 10686 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h

Macro Definition Documentation#

sl_btmesh_evt_mbt_client_server_failed_id#

#define sl_btmesh_evt_mbt_client_server_failed_id
Value:
0x0b2800a8

Identifier of the server_failed event.


Definition at line 10673 of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h