sl_btmesh_evt_mbt_client_start_transfer_complete#
Transfer start is complete.
All active servers have responded to the transfer start command. The first block start should be initiated with sl_btmesh_mbt_client_start_block.
Modules#
sl_btmesh_evt_mbt_client_start_transfer_complete_s
Typedefs#
Macros#
#define
Identifier of the start_transfer_complete event.
Typedef Documentation#
sl_btmesh_evt_mbt_client_start_transfer_complete_t#
typedef struct sl_btmesh_evt_mbt_client_start_transfer_complete_s sl_btmesh_evt_mbt_client_start_transfer_complete_t
Definition at line
10452
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_mbt_client_start_transfer_complete_id#
#define sl_btmesh_evt_mbt_client_start_transfer_complete_idValue:
0x052800a8
Identifier of the start_transfer_complete event.
Definition at line
10442
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h