sl_btmesh_evt_mbt_client_tx_complete#
Previous command has been transmitted to all recipients.
When the previous command has been transmitted to all MBT Servers, either multicasting or unicasting to each server one by one, this event indicates that the whole transmission is completed. It may be used for timing retries, in case all servers do not respond within an expected time after this event.
Modules#
sl_btmesh_evt_mbt_client_tx_complete_s
Typedefs#
Macros#
#define
sl_btmesh_evt_mbt_client_tx_complete_id 0x0a2800a8
Identifier of the tx_complete event.
Typedef Documentation#
sl_btmesh_evt_mbt_client_tx_complete_t#
typedef struct sl_btmesh_evt_mbt_client_tx_complete_s sl_btmesh_evt_mbt_client_tx_complete_t
Definition at line
10659
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h
Macro Definition Documentation#
sl_btmesh_evt_mbt_client_tx_complete_id#
#define sl_btmesh_evt_mbt_client_tx_complete_idValue:
0x0a2800a8
Identifier of the tx_complete event.
Definition at line
10649
of file /mnt/raid/workspaces/ws.nQlGxFofL/overlay/gsdk/protocol/bluetooth/build/native/mesh_app/inc/sl_btmesh_api.h