Functions and definitions specific to the breakout board. More...

Macros

#define halInternalInitRadioHoldOff ()
Radio HoldOff not supported. More...
#define halInternalPowerUpBoard ()
#define halInternalPowerDownBoard ()
#define DEFINE_SPI_CONFIG_VARIABLES ()
Initialize GPIO powerup configuration variables. More...
#define COM_RETARGET_SERIAL

Packet Trace

PRO2+ SPI-Master configuration

When PACKET_TRACE is defined, ::GPIO_PACFGH will automatically be setup by halInit() to enable Packet Trace support on PA4 and PA5, in addition to the configuration specified below.

Note
This define will override any settings for PA4 and PA5.
#define PACKET_TRACE
This define does not equate to anything. It is used as a trigger to enable Packet Trace support on the breakout board (dev0680). More...

Detailed Description

Functions and definitions specific to the breakout board.

Macro Definition Documentation

#define COM_RETARGET_SERIAL

GPIO definitions for WSTK BC serial Initialize GPIOs direction and default state for VCP.

Definition at line 119 of file ezr32.h .

#define DEFINE_SPI_CONFIG_VARIABLES ( )

Initialize GPIO powerup configuration variables.

Definition at line 81 of file ezr32.h .

#define halInternalInitRadioHoldOff ( )

Radio HoldOff not supported.

Definition at line 64 of file ezr32.h .

#define halInternalPowerDownBoard ( )

Definition at line 72 of file ezr32.h .

#define halInternalPowerUpBoard ( )

Definition at line 66 of file ezr32.h .

#define PACKET_TRACE

This define does not equate to anything. It is used as a trigger to enable Packet Trace support on the breakout board (dev0680).

Definition at line 59 of file ezr32.h .