Functions | |
void | emberAfPluginPollSetShortPollInterval (uint8_t intervalQS) |
Sets the short poll interval. More... | |
void | emberAfPluginPollSetLongPollInterval (uint16_t intervalS) |
Sets the long poll interval. More... | |
void | emberAfPluginPollEnableShortPolling (bool enable) |
Enables/disables short polling. More... | |
Detailed Description
See poll.h
for source code.
Function Documentation
void emberAfPluginPollEnableShortPolling | ( | bool | enable | ) |
Enables/disables short polling.
- Parameters
-
enable
If this parameter is true, short polling is enabled. Otherwise, the node switches back to long polling.
void emberAfPluginPollSetLongPollInterval | ( | uint16_t | intervalS | ) |
Sets the long poll interval.
- Parameters
-
intervalS
The long poll interval in seconds.
void emberAfPluginPollSetShortPollInterval | ( | uint8_t | intervalQS | ) |
Sets the short poll interval.
- Parameters
-
intervalQS
The short poll interval in quarter seconds.