EmberNetworkParameters Struct Reference
Holds network parameters. More...
#include <
ember-types.h
>
Data Fields | |
uint16_t | panId |
int8_t | radioTxPower |
uint8_t | radioChannel |
Holds network parameters.
For information about power settings and radio channels, see the technical specification for the RF communication module in your Developer Kit.
Definition at line 142
of file ember-types.h
.
Field Documentation
uint16_t EmberNetworkParameters::panId |
The network's PAN identifier.
Definition at line 144
of file ember-types.h
.
uint8_t EmberNetworkParameters::radioChannel |
A radio channel. Be sure to specify a channel supported by the radio.
Definition at line 148
of file ember-types.h
.
int8_t EmberNetworkParameters::radioTxPower |
A power setting, in dBm.
Definition at line 146
of file ember-types.h
.
The documentation for this struct was generated from the following file:
ember-types.h