EmberMacFrame Struct Reference
A structure that describes the addressing fields of a 802.15.4 frame. More...
#include <
ember-types.h
>
Data Fields | |
EmberMacAddress | srcAddress |
EmberMacAddress | dstAddress |
EmberPanId | srcPanId |
EmberPanId | dstPanId |
bool | srcPanIdSpecified |
bool | dstPanIdSpecified |
A structure that describes the addressing fields of a 802.15.4 frame.
Definition at line 300
of file ember-types.h
.
Field Documentation
EmberMacAddress EmberMacFrame::dstAddress |
An EmberMacAddress structure indicating the destination address of a MAC frame.
Definition at line 309
of file ember-types.h
.
EmberPanId EmberMacFrame::dstPanId |
An EmberPanId struct indicating the destination PAN ID of a MAC frame. This field is meaningful only if dstPanIdSpecified is set to true.
Definition at line 319
of file ember-types.h
.
bool EmberMacFrame::dstPanIdSpecified |
True if the dstPanId field is set, false otherwise.
Definition at line 327
of file ember-types.h
.
EmberMacAddress EmberMacFrame::srcAddress |
An EmberMacAddress structure indicating the source address of a MAC frame.
Definition at line 304
of file ember-types.h
.
EmberPanId EmberMacFrame::srcPanId |
An EmberPanId struct indicating the source PAN ID of a MAC frame. This field is meaningful only if srcPanIdSpecified is set to true.
Definition at line 314
of file ember-types.h
.
bool EmberMacFrame::srcPanIdSpecified |
True if the srcPanId field is set, false otherwise.
Definition at line 323
of file ember-types.h
.
The documentation for this struct was generated from the following file:
ember-types.h