|
uint16_t | NTOHS (uint16_t val) |
| Converts a short (16-bit) value from network to host byte order. More...
|
|
uint32_t | NTOHL (uint32_t val) |
| Converts a long (32-bit) value from network to host byte order. More...
|
|
uint32_t | SwapEndiannessInt32u (uint32_t val) |
|
*/
Functions that provide conversions from network to host byte order. Network byte order is big endian, so these APIs are only necessary on platforms which have a natural little endian byte order. On big-endian platforms, the APIs are macro'd away to nothing. See endian.h
for source code.
Definition at line 61
of file endian.h
.
Definition at line 64
of file endian.h
.
uint32_t NTOHL |
( |
uint32_t |
val | ) |
|
Converts a long (32-bit) value from network to host byte order.
uint16_t NTOHS |
( |
uint16_t |
val | ) |
|
Converts a short (16-bit) value from network to host byte order.
uint32_t SwapEndiannessInt32u |
( |
uint32_t |
val | ) |
|