EmberEventData_S Struct Reference
Complete events with a control and a handler procedure. More...
#include <
ember-types.h
>
Data Fields | |
EmberEventControl * | control |
void(* | handler )(void) |
Complete events with a control and a handler procedure.
An application typically creates an array of events along with their handlers. The main loop passes the array to emberRunEvents() to call the handlers of any events whose time has arrived.
Definition at line 510
of file ember-types.h
.
Field Documentation
EmberEventControl* EmberEventData_S::control |
The control structure for the event.
Definition at line 512
of file ember-types.h
.
void(* EmberEventData_S::handler) (void) |
The procedure to call when the event fires.
Definition at line 514
of file ember-types.h
.
The documentation for this struct was generated from the following file:
ember-types.h