WSTK Sensors Plugin
Functions | |
EmberStatus | emberAfPluginWstkSensorsGetSample (uint32_t *rhData, int32_t *tData) |
Reads a sample of the temperature and relative humidity values from the WSTK Si7013 sensors. More... | |
Detailed Description
See wstk-sensors.h
for source code.
Function Documentation
EmberStatus emberAfPluginWstkSensorsGetSample |
( | uint32_t * | rhData, |
int32_t * | tData |
||
) |
Reads a sample of the temperature and relative humidity values from the WSTK Si7013 sensors.
- Parameters
-
rhData
A pointer to a 32-bit unsigned integer where the relative humidity sample is written. tData
A pointer to a 32-bit signed integer where the temperature is written. Temperature is sampled in "millicelsius".
- Returns
- An EmberStatus value of EMBER_SUCCESS if the relative humidity and temperature sample were successfully read from the Si7013 sensors. Otherwise, an EmberStatus value of EMBER_ERR_FATAL.