EmberMacAddress Struct Reference
A structure that stores an 802.15.4 address. More...
#include <
ember-types.h
>
Data Fields | |
union { | |
uint8_t longAddress [EUI64_SIZE] | |
uint16_t shortAddress | |
} | addr |
EmberMacAddressMode | mode |
A structure that stores an 802.15.4 address.
Definition at line 287
of file ember-types.h
.
Field Documentation
union { ... } EmberMacAddress::addr |
uint8_t EmberMacAddress::longAddress[EUI64_SIZE] |
Definition at line 289
of file ember-types.h
.
EmberMacAddressMode EmberMacAddress::mode |
Definition at line 293
of file ember-types.h
.
uint16_t EmberMacAddress::shortAddress |
Definition at line 290
of file ember-types.h
.
The documentation for this struct was generated from the following file:
ember-types.h