Data Structures
Here are the data structures with brief descriptions:
EmberCommandEntry | Command entry for a command table |
EmberCommandState | For use when declaring a separate command streams. The fields are not accessed directly by the application |
EmberEventControl | Control structure for events |
EmberEventData_S | Complete events with a control and a handler procedure |
EmberIncomingMacMessage | An instance of this structure is passed to emberIncomingMacMessageHandler(). It describes the incoming MAC frame |
EmberIncomingMessage | An instance of this structure is passed to emberIncomingMessageHandler(). It describes the incoming message |
EmberKeyData | This data structure contains the security key, most prominently used by emberSetSecurityKey |
EmberMacAddress | A structure that stores an 802.15.4 address |
EmberMacFrame | A structure that describes the addressing fields of a 802.15.4 frame |
EmberNetworkParameters | Hold network parameters |
EmberOutgoingMacMessage | An instance of this structure is passed to emberMacMessageSentHandler(). It describes the outgoing MAC frame |
EmberOutgoingMessage | An instance of this structure is passed to emberMessageSentHandler(). It describes the outgoing packet |
EmberTaskControl | Control structure for tasks |
Event_s | |
EventActions | The static part of an event. Each event can be used with only one event queue |
EventQueue_s | An event queue is currently just a list of events ordered by execution time |
RTCCRamData | |
tokTypeStackChildTableEntry | Type of an element of TOKEN_STACK_CHILD_TABLE (indexed token). Keeps children information of a device, which has parent support enabled |
tokTypeStackKey | Type for TOKEN_STACK_NVDATA_VERSION. Keeps the version number of stack tokens |
tokTypeStackNodeData | Type for TOKEN_STACK_NODE_DATA. Generic information of the node is stored in this token |