IAR PLATFORM_HEADER Configuration
Compiler and Platform specific definitions and typedefs for the IAR ARM C compiler. More...
Macros |
|
| #define | HAL_HAS_INT64 |
|
Denotes that this platform supports 64-bit data-types.
More...
|
|
| #define | _HAL_USE_COMMON_PGM_ |
Use the Master Program Memory Declarations from
platform-common.h
.
More...
|
|
| #define | _HAL_USE_COMMON_MEMUTILS_ |
|
If the line below is uncommented we will use Ember memory APIs, otherwise, we will use the C Standard library (memset,memcpy,memmove) APIs.
More...
|
|
| #define | PLATCOMMONOKTOINCLUDE |
Include
platform-common.h
last to pick up defaults and common definitions.
More...
|
|
| #define | MAIN_FUNCTION_PARAMETERS void |
|
The kind of arguments the main function takes.
More...
|
|
| #define | MAIN_FUNCTION_ARGUMENTS |
Functions |
|
| void | _executeBarrierInstructions (void) |
Master Variable Types |
|
|
These are a set of typedefs to make the size of all variable declarations explicitly known. |
|
| typedef bool | boolean |
|
A typedef to make the size of the variable explicitly known.
More...
|
|
| typedef unsigned char | int8u |
|
A typedef to make the size of the variable explicitly known.
More...
|
|
| typedef signed char | int8s |
|
A typedef to make the size of the variable explicitly known.
More...
|
|
| typedef unsigned short | int16u |
|
A typedef to make the size of the variable explicitly known.
More...
|
|
| typedef signed short | int16s |
|
A typedef to make the size of the variable explicitly known.
More...
|
|
| typedef unsigned int | int32u |
|
A typedef to make the size of the variable explicitly known.
More...
|
|
| typedef signed int | int32s |
|
A typedef to make the size of the variable explicitly known.
More...
|
|
| typedef unsigned long long | int64u |
|
A typedef to make the size of the variable explicitly known.
More...
|
|
| typedef signed long long | int64s |
|
A typedef to make the size of the variable explicitly known.
More...
|
|
| typedef unsigned int | PointerType |
|
A typedef to make the size of the variable explicitly known.
More...
|
|
Miscellaneous Macros |
|
| void | halInternalAssertFailed (const char *filename, int linenumber) |
A prototype definition for use by the assert macro. (see
hal/micro/micro.h
)
More...
|
|
| void | halInternalResetWatchDog (void) |
|
Macro to reset the watchdog timer. Note: be very very careful when using this as you can easily get into an infinite loop if you are not careful.
More...
|
|
| #define | BIGENDIAN_CPU false |
|
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
More...
|
|
| #define | NTOHS (val) (__REV16(val)) |
|
Define intrinsics for NTOHL and NTOHS to save code space by making endian.c compile to nothing.
More...
|
|
| #define | NTOHL (val) (__REV(val)) |
|
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
More...
|
|
| #define | NO_STRIPPING __root |
|
A friendlier name for the compiler's intrinsic for not stripping.
More...
|
|
| #define | EEPROM errorerror |
|
A friendlier name for the compiler's intrinsic for eeprom reference.
More...
|
|
| #define | __SOURCEFILE__ __FILE__ |
|
The
SOURCEFILE
macro is used by asserts to list the filename if it isn't otherwise defined, set it to the compiler intrinsic which specifies the whole filename and path of the sourcefile.
More...
|
|
| #define | assert (condition) |
A custom implementation of the C language assert macro. This macro implements the conditional evaluation and calls the function
halInternalAssertFailed()
. (see
hal/micro/micro.h
)
More...
|
|
| #define | halResetWatchdog () halInternalResetWatchDog () |
|
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
More...
|
|
| #define | UNUSED |
|
Declare a variable as unused to avoid a warning. Has no effect in IAR builds.
More...
|
|
| #define | SIGNED_ENUM |
|
Some platforms need to cast enum values that have the high bit set.
More...
|
|
| #define | STACK_FILL_VALUE 0xCDCDCDCDU |
|
Define the magic value that is interpreted by IAR C-SPY's Stack View.
More...
|
|
| #define | RAMFUNC __ramfunc |
|
Define a generic RAM function identifier to a compiler specific one.
More...
|
|
| #define | NO_OPERATION () __no_operation() |
|
Define a generic no operation identifier to a compiler specific one.
More...
|
|
| #define | SET_REG_FIELD (reg, field, value) |
|
A convenience macro that makes it easy to change the field of a register to any unsigned value.
More...
|
|
| #define | SET_CMSIS_REG (reg, mask, value) |
|
A convenience macro that makes it easy to change a register using the provided mask(s) and value(s). Example: SET_CMSIS_REG(GPIO->P[1].CFGH, (_GPIO_P_CFGH_Px5_MASK | _GPIO_P_CFGH_Px6_MASK), (GPIO_P_CFGH_Px5_OUT | GPIO_P_CFGH_Px6_OUT));.
More...
|
|
| #define | SET_CMSIS_REG_FIELD (reg, field, value) |
|
A convenience macro that makes it easy to change the field of a register, as defined in CMSIS Device headers, to any unsigned value. Example using EM35xx: SET_CMSIS_REG_FIELD(GPIO->P[0].CFGL, GPIO_P_CFGL_Px0, _GPIO_P_CFGL_Px0_OUT);.
More...
|
|
| #define | simulatedTimePasses () |
|
Stub for code not running in simulation.
More...
|
|
| #define | simulatedTimePassesMs (x) |
|
Stub for code not running in simulation.
More...
|
|
| #define | simulatedSerialTimePasses () |
|
Stub for code not running in simulation.
More...
|
|
| #define | _HAL_USE_COMMON_DIVMOD_ |
Use the Divide and Modulus Operations from
platform-common.h
.
More...
|
|
| #define | VAR_AT_SEGMENT (__variableDeclaration, __segmentName) __variableDeclaration @ __segmentName |
|
Provide a portable way to specify the segment where a variable lives.
More...
|
|
| #define | STRINGIZE (X) #X |
|
Convinience macro for turning a token into a string.
More...
|
|
| #define | ALIGNMENT (X) _Pragma( STRINGIZE (data_alignment = X)) |
|
Provide a portable way to align data.
More...
|
|
| #define | WEAK (__symbol) __weak __symbol |
|
Provide a portable way to specify a symbol as weak.
More...
|
|
| #define | NO_INIT (__symbol) __no_init __symbol |
|
Provide a portable way to specify a non initialized symbol.
More...
|
|
| #define | STATIC_ASSERT (__condition, __errorstr) static_assert(__condition, __errorstr) |
|
Provide a portable way to specify a compile time assert.
More...
|
|
Portable segment names |
|
| #define | __NO_INIT__ ".noinit" |
|
Portable segment names.
More...
|
|
| #define | __DEBUG_CHANNEL__ "DEBUG_CHANNEL" |
|
Portable segment names.
More...
|
|
| #define | __INTVEC__ ".intvec" |
|
Portable segment names.
More...
|
|
| #define | __CSTACK__ "CSTACK" |
|
Portable segment names.
More...
|
|
| #define | __RESETINFO__ "RESETINFO" |
|
Portable segment names.
More...
|
|
| #define | __DATA_INIT__ ".data_init" |
|
Portable segment names.
More...
|
|
| #define | __DATA__ ".data" |
|
Portable segment names.
More...
|
|
| #define | __BSS__ ".bss" |
|
Portable segment names.
More...
|
|
| #define | __CONST__ ".rodata" |
|
Portable segment names.
More...
|
|
| #define | __TEXT__ ".text" |
|
Portable segment names.
More...
|
|
| #define | __TEXTRW_INIT__ ".textrw_init" |
|
Portable segment names.
More...
|
|
| #define | __TEXTRW__ ".textrw" |
|
Portable segment names.
More...
|
|
| #define | __AAT__ "AAT" |
|
Portable segment names.
More...
|
|
| #define | __BAT__ "BAT" |
|
Portable segment names.
More...
|
|
| #define | __BAT_INIT__ "BAT" |
|
Portable segment names.
More...
|
|
| #define | __FAT__ "FAT" |
|
Portable segment names.
More...
|
|
| #define | __RAT__ "RAT" |
|
Portable segment names.
More...
|
|
| #define | __SIMEE__ "SIMEE" |
|
Portable segment names.
More...
|
|
| #define | __PSSTORE__ "PSSTORE" |
|
Portable segment names.
More...
|
|
| #define | __LONGTOKEN__ "LONGTOKEN" |
|
Portable segment names.
More...
|
|
| #define | __EMHEAP__ "EMHEAP" |
|
Portable segment names.
More...
|
|
| #define | __GUARD_REGION__ "GUARD_REGION" |
|
Portable segment names.
More...
|
|
| #define | __DLIB_PERTHREAD_INIT__ "__DLIB_PERTHREAD_init" |
|
Portable segment names.
More...
|
|
| #define | __DLIB_PERTHREAD_INITIALIZED_DATA__ "DLIB_PERTHREAD_INITIALIZED_DATA" |
|
Portable segment names.
More...
|
|
| #define | __DLIB_PERTHREAD_ZERO_DATA__ "DLIB_PERTHREAD_ZERO_DATA" |
|
Portable segment names.
More...
|
|
| #define | __INTERNAL_STORAGE__ "INTERNAL_STORAGE" |
|
Portable segment names.
More...
|
|
| #define | __LOCKBITS_IN_MAINFLASH__ "LOCKBITS_IN_MAINFLASH" |
|
Portable segment names.
More...
|
|
| #define | __UNRETAINED_RAM__ "UNRETAINED_RAM" |
|
Portable segment names.
More...
|
|
| #define | _NO_INIT_SEGMENT_BEGIN __segment_begin( __NO_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _DEBUG_CHANNEL_SEGMENT_BEGIN __segment_begin( __DEBUG_CHANNEL__ ) |
|
Portable segment names.
More...
|
|
| #define | _INTVEC_SEGMENT_BEGIN __segment_begin( __INTVEC__ ) |
|
Portable segment names.
More...
|
|
| #define | _CSTACK_SEGMENT_BEGIN __segment_begin( __CSTACK__ ) |
|
Portable segment names.
More...
|
|
| #define | _RESETINFO_SEGMENT_BEGIN __segment_begin( __RESETINFO__ ) |
|
Portable segment names.
More...
|
|
| #define | _DATA_INIT_SEGMENT_BEGIN __segment_begin( __DATA_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _DATA_SEGMENT_BEGIN __segment_begin( __DATA__ ) |
|
Portable segment names.
More...
|
|
| #define | _BSS_SEGMENT_BEGIN __segment_begin( __BSS__ ) |
|
Portable segment names.
More...
|
|
| #define | _CONST_SEGMENT_BEGIN __segment_begin( __CONST__ ) |
|
Portable segment names.
More...
|
|
| #define | _TEXT_SEGMENT_BEGIN __segment_begin( __TEXT__ ) |
|
Portable segment names.
More...
|
|
| #define | _TEXTRW_INIT_SEGMENT_BEGIN __segment_begin( __TEXTRW_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _TEXTRW_SEGMENT_BEGIN __segment_begin( __TEXTRW__ ) |
|
Portable segment names.
More...
|
|
| #define | _AAT_SEGMENT_BEGIN __segment_begin( __AAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _BAT_SEGMENT_BEGIN __segment_begin( __BAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _BAT_INIT_SEGMENT_BEGIN __segment_begin( __BAT_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _FAT_SEGMENT_BEGIN __segment_begin( __FAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _RAT_SEGMENT_BEGIN __segment_begin( __RAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _SIMEE_SEGMENT_BEGIN __segment_begin( __SIMEE__ ) |
|
Portable segment names.
More...
|
|
| #define | _PSSTORE_SEGMENT_BEGIN __segment_begin( __PSSTORE__ ) |
|
Portable segment names.
More...
|
|
| #define | _LONGTOKEN_SEGMENT_BEGIN __segment_begin( __LONGTOKEN__ ) |
|
Portable segment names.
More...
|
|
| #define | _EMHEAP_SEGMENT_BEGIN __segment_begin( __EMHEAP__ ) |
|
Portable segment names.
More...
|
|
| #define | _GUARD_REGION_SEGMENT_BEGIN __segment_begin( __GUARD_REGION__ ) |
|
Portable segment names.
More...
|
|
| #define | _DLIB_PERTHREAD_INIT_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_INITIALIZED_DATA__ ) |
|
Portable segment names.
More...
|
|
| #define | _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_ZERO_DATA__ ) |
|
Portable segment names.
More...
|
|
| #define | _INTERNAL_STORAGE_SEGMENT_BEGIN __segment_begin( __INTERNAL_STORAGE__ ) |
|
Portable segment names.
More...
|
|
| #define | _LOCKBITS_IN_MAINFLASH_SEGMENT_BEGIN __segment_begin( __LOCKBITS_IN_MAINFLASH__ ) |
|
Portable segment names.
More...
|
|
| #define | _UNRETAINED_RAM_SEGMENT_BEGIN __segment_begin( __UNRETAINED_RAM__ ) |
|
Portable segment names.
More...
|
|
| #define | _NO_INIT_SEGMENT_END __segment_end( __NO_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _DEBUG_CHANNEL_SEGMENT_END __segment_end( __DEBUG_CHANNEL__ ) |
|
Portable segment names.
More...
|
|
| #define | _INTVEC_SEGMENT_END __segment_end( __INTVEC__ ) |
|
Portable segment names.
More...
|
|
| #define | _CSTACK_SEGMENT_END __segment_end( __CSTACK__ ) |
|
Portable segment names.
More...
|
|
| #define | _RESETINFO_SEGMENT_END __segment_end( __RESETINFO__ ) |
|
Portable segment names.
More...
|
|
| #define | _DATA_INIT_SEGMENT_END __segment_end( __DATA_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _DATA_SEGMENT_END __segment_end( __DATA__ ) |
|
Portable segment names.
More...
|
|
| #define | _BSS_SEGMENT_END __segment_end( __BSS__ ) |
|
Portable segment names.
More...
|
|
| #define | _CONST_SEGMENT_END __segment_end( __CONST__ ) |
|
Portable segment names.
More...
|
|
| #define | _TEXT_SEGMENT_END __segment_end( __TEXT__ ) |
|
Portable segment names.
More...
|
|
| #define | _TEXTRW_INIT_SEGMENT_END __segment_end( __TEXTRW_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _TEXTRW_SEGMENT_END __segment_end( __TEXTRW__ ) |
|
Portable segment names.
More...
|
|
| #define | _AAT_SEGMENT_END __segment_end( __AAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _BAT_SEGMENT_END __segment_end( __BAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _BAT_INIT_SEGMENT_END __segment_end( __BAT_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _FAT_SEGMENT_END __segment_end( __FAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _RAT_SEGMENT_END __segment_end( __RAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _SIMEE_SEGMENT_END __segment_end( __SIMEE__ ) |
|
Portable segment names.
More...
|
|
| #define | _PSSTORE_SEGMENT_END __segment_end( __PSSTORE__ ) |
|
Portable segment names.
More...
|
|
| #define | _LONGTOKEN_SEGMENT_END __segment_end( __LONGTOKEN__ ) |
|
Portable segment names.
More...
|
|
| #define | _EMHEAP_SEGMENT_END __segment_end( __EMHEAP__ ) |
|
Portable segment names.
More...
|
|
| #define | _GUARD_REGION_SEGMENT_END __segment_end( __GUARD_REGION__ ) |
|
Portable segment names.
More...
|
|
| #define | _DLIB_PERTHREAD_INIT_SEGMENT_END __segment_end( __DLIB_PERTHREAD_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_END __segment_end( __DLIB_PERTHREAD_INITIALIZED_DATA__ ) |
|
Portable segment names.
More...
|
|
| #define | _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_END __segment_end( __DLIB_PERTHREAD_ZERO_DATA__ ) |
|
Portable segment names.
More...
|
|
| #define | _INTERNAL_STORAGE_SEGMENT_END __segment_end( __INTERNAL_STORAGE__ ) |
|
Portable segment names.
More...
|
|
| #define | _LOCKBITS_IN_MAINFLASH_SEGMENT_END __segment_end( __LOCKBITS_IN_MAINFLASH__ ) |
|
Portable segment names.
More...
|
|
| #define | _UNRETAINED_RAM_SEGMENT_END __segment_end( __UNRETAINED_RAM__ ) |
|
Portable segment names.
More...
|
|
| #define | _NO_INIT_SEGMENT_SIZE __segment_size( __NO_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _DEBUG_CHANNEL_SEGMENT_SIZE __segment_size( __DEBUG_CHANNEL__ ) |
|
Portable segment names.
More...
|
|
| #define | _INTVEC_SEGMENT_SIZE __segment_size( __INTVEC__ ) |
|
Portable segment names.
More...
|
|
| #define | _CSTACK_SEGMENT_SIZE __segment_size( __CSTACK__ ) |
|
Portable segment names.
More...
|
|
| #define | _RESETINFO_SEGMENT_SIZE __segment_size( __RESETINFO__ ) |
|
Portable segment names.
More...
|
|
| #define | _DATA_INIT_SEGMENT_SIZE __segment_size( __DATA_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _DATA_SEGMENT_SIZE __segment_size( __DATA__ ) |
|
Portable segment names.
More...
|
|
| #define | _BSS_SEGMENT_SIZE __segment_size( __BSS__ ) |
|
Portable segment names.
More...
|
|
| #define | _CONST_SEGMENT_SIZE __segment_size( __CONST__ ) |
|
Portable segment names.
More...
|
|
| #define | _TEXT_SEGMENT_SIZE __segment_size( __TEXT__ ) |
|
Portable segment names.
More...
|
|
| #define | _TEXTRW_INIT_SEGMENT_SIZE __segment_size( __TEXTRW_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _TEXTRW_SEGMENT_SIZE __segment_size( __TEXTRW__ ) |
|
Portable segment names.
More...
|
|
| #define | _AAT_SEGMENT_SIZE __segment_size( __AAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _BAT_SEGMENT_SIZE __segment_size( __BAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _BAT_INIT_SEGMENT_SIZE __segment_size( __BAT_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _FAT_SEGMENT_SIZE __segment_size( __FAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _RAT_SEGMENT_SIZE __segment_size( __RAT__ ) |
|
Portable segment names.
More...
|
|
| #define | _SIMEE_SEGMENT_SIZE __segment_size( __SIMEE__ ) |
|
Portable segment names.
More...
|
|
| #define | _PSSTORE_SEGMENT_SIZE __segment_size( __PSSTORE__ ) |
|
Portable segment names.
More...
|
|
| #define | _LONGTOKEN_SEGMENT_SIZE __segment_size( __LONGTOKEN__ ) |
|
Portable segment names.
More...
|
|
| #define | _EMHEAP_SEGMENT_SIZE __segment_size( __EMHEAP__ ) |
|
Portable segment names.
More...
|
|
| #define | _GUARD_REGION_SEGMENT_SIZE __segment_size( __GUARD_REGION__ ) |
|
Portable segment names.
More...
|
|
| #define | _DLIB_PERTHREAD_INIT_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_INIT__ ) |
|
Portable segment names.
More...
|
|
| #define | _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_INITIALIZED_DATA__ ) |
|
Portable segment names.
More...
|
|
| #define | _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_ZERO_DATA__ ) |
|
Portable segment names.
More...
|
|
| #define | _INTERNAL_STORAGE_SEGMENT_SIZE __segment_size( __INTERNAL_STORAGE__ ) |
|
Portable segment names.
More...
|
|
| #define | _LOCKBITS_IN_MAINFLASH_SEGMENT_SIZE __segment_size( __LOCKBITS_IN_MAINFLASH__ ) |
|
Portable segment names.
More...
|
|
| #define | _UNRETAINED_RAM_SEGMENT_SIZE __segment_size( __UNRETAINED_RAM__ ) |
|
Portable segment names.
More...
|
|
External Declarations |
|
|
These are routines that are defined in certain header files that we don't want to include, e.g. stdlib.h |
|
| int | abs (int I) |
|
Returns the absolute value of I (also called the magnitude of I). That is, if I is negative, the result is the opposite of I, but if I is nonnegative the result is I.
More...
|
|
Detailed Description
Compiler and Platform specific definitions and typedefs for the IAR ARM C compiler.
- Note
-
iar.hshould be included first in all source files by setting the preprocessor macro PLATFORM_HEADER to point to it.iar.hautomatically includesplatform-common.h.
See
iar.h
and
platform-common.h
for source code.
Macro Definition Documentation
◆ __AAT__
| #define __AAT__ "AAT" |
Portable segment names.
Definition at line
368
of file
iar.h
.
◆ __BAT__
| #define __BAT__ "BAT" |
Portable segment names.
Definition at line
369
of file
iar.h
.
◆ __BAT_INIT__
| #define __BAT_INIT__ "BAT" |
Portable segment names.
Definition at line
370
of file
iar.h
.
◆ __BSS__
| #define __BSS__ ".bss" |
Portable segment names.
Definition at line
363
of file
iar.h
.
◆ __CONST__
| #define __CONST__ ".rodata" |
Portable segment names.
Definition at line
364
of file
iar.h
.
◆ __CSTACK__
| #define __CSTACK__ "CSTACK" |
Portable segment names.
Definition at line
359
of file
iar.h
.
◆ __DATA__
| #define __DATA__ ".data" |
Portable segment names.
Definition at line
362
of file
iar.h
.
◆ __DATA_INIT__
| #define __DATA_INIT__ ".data_init" |
Portable segment names.
Definition at line
361
of file
iar.h
.
◆ __DEBUG_CHANNEL__
| #define __DEBUG_CHANNEL__ "DEBUG_CHANNEL" |
Portable segment names.
Definition at line
357
of file
iar.h
.
◆ __DLIB_PERTHREAD_INIT__
| #define __DLIB_PERTHREAD_INIT__ "__DLIB_PERTHREAD_init" |
Portable segment names.
Definition at line
378
of file
iar.h
.
◆ __DLIB_PERTHREAD_INITIALIZED_DATA__
| #define __DLIB_PERTHREAD_INITIALIZED_DATA__ "DLIB_PERTHREAD_INITIALIZED_DATA" |
Portable segment names.
Definition at line
379
of file
iar.h
.
◆ __DLIB_PERTHREAD_ZERO_DATA__
| #define __DLIB_PERTHREAD_ZERO_DATA__ "DLIB_PERTHREAD_ZERO_DATA" |
Portable segment names.
Definition at line
380
of file
iar.h
.
◆ __EMHEAP__
| #define __EMHEAP__ "EMHEAP" |
Portable segment names.
Definition at line
376
of file
iar.h
.
◆ __FAT__
| #define __FAT__ "FAT" |
Portable segment names.
Definition at line
371
of file
iar.h
.
◆ __GUARD_REGION__
| #define __GUARD_REGION__ "GUARD_REGION" |
Portable segment names.
Definition at line
377
of file
iar.h
.
◆ __INTERNAL_STORAGE__
| #define __INTERNAL_STORAGE__ "INTERNAL_STORAGE" |
Portable segment names.
Definition at line
381
of file
iar.h
.
◆ __INTVEC__
| #define __INTVEC__ ".intvec" |
Portable segment names.
Definition at line
358
of file
iar.h
.
◆ __LOCKBITS_IN_MAINFLASH__
| #define __LOCKBITS_IN_MAINFLASH__ "LOCKBITS_IN_MAINFLASH" |
Portable segment names.
Definition at line
382
of file
iar.h
.
◆ __LONGTOKEN__
| #define __LONGTOKEN__ "LONGTOKEN" |
Portable segment names.
Definition at line
375
of file
iar.h
.
◆ __NO_INIT__
| #define __NO_INIT__ ".noinit" |
Portable segment names.
Definition at line
356
of file
iar.h
.
◆ __PSSTORE__
| #define __PSSTORE__ "PSSTORE" |
Portable segment names.
Definition at line
374
of file
iar.h
.
◆ __RAT__
| #define __RAT__ "RAT" |
Portable segment names.
Definition at line
372
of file
iar.h
.
◆ __RESETINFO__
| #define __RESETINFO__ "RESETINFO" |
Portable segment names.
Definition at line
360
of file
iar.h
.
◆ __SIMEE__
| #define __SIMEE__ "SIMEE" |
Portable segment names.
Definition at line
373
of file
iar.h
.
◆ __SOURCEFILE__
| #define __SOURCEFILE__ __FILE__ |
The SOURCEFILE macro is used by asserts to list the filename if it isn't otherwise defined, set it to the compiler intrinsic which specifies the whole filename and path of the sourcefile.
Definition at line
167
of file
iar.h
.
◆ __TEXT__
| #define __TEXT__ ".text" |
Portable segment names.
Definition at line
365
of file
iar.h
.
◆ __TEXTRW__
| #define __TEXTRW__ ".textrw" |
Portable segment names.
Definition at line
367
of file
iar.h
.
◆ __TEXTRW_INIT__
| #define __TEXTRW_INIT__ ".textrw_init" |
Portable segment names.
Definition at line
366
of file
iar.h
.
◆ __UNRETAINED_RAM__
| #define __UNRETAINED_RAM__ "UNRETAINED_RAM" |
Portable segment names.
Definition at line
383
of file
iar.h
.
◆ _AAT_SEGMENT_BEGIN
| #define _AAT_SEGMENT_BEGIN __segment_begin( __AAT__ ) |
Portable segment names.
Definition at line
433
of file
iar.h
.
◆ _AAT_SEGMENT_END
| #define _AAT_SEGMENT_END __segment_end( __AAT__ ) |
Portable segment names.
Definition at line
462
of file
iar.h
.
◆ _AAT_SEGMENT_SIZE
| #define _AAT_SEGMENT_SIZE __segment_size( __AAT__ ) |
Portable segment names.
Definition at line
491
of file
iar.h
.
◆ _BAT_INIT_SEGMENT_BEGIN
| #define _BAT_INIT_SEGMENT_BEGIN __segment_begin( __BAT_INIT__ ) |
Portable segment names.
Definition at line
435
of file
iar.h
.
◆ _BAT_INIT_SEGMENT_END
| #define _BAT_INIT_SEGMENT_END __segment_end( __BAT_INIT__ ) |
Portable segment names.
Definition at line
464
of file
iar.h
.
◆ _BAT_INIT_SEGMENT_SIZE
| #define _BAT_INIT_SEGMENT_SIZE __segment_size( __BAT_INIT__ ) |
Portable segment names.
Definition at line
493
of file
iar.h
.
◆ _BAT_SEGMENT_BEGIN
| #define _BAT_SEGMENT_BEGIN __segment_begin( __BAT__ ) |
Portable segment names.
Definition at line
434
of file
iar.h
.
◆ _BAT_SEGMENT_END
| #define _BAT_SEGMENT_END __segment_end( __BAT__ ) |
Portable segment names.
Definition at line
463
of file
iar.h
.
◆ _BAT_SEGMENT_SIZE
| #define _BAT_SEGMENT_SIZE __segment_size( __BAT__ ) |
Portable segment names.
Definition at line
492
of file
iar.h
.
◆ _BSS_SEGMENT_BEGIN
| #define _BSS_SEGMENT_BEGIN __segment_begin( __BSS__ ) |
Portable segment names.
Definition at line
428
of file
iar.h
.
◆ _BSS_SEGMENT_END
| #define _BSS_SEGMENT_END __segment_end( __BSS__ ) |
Portable segment names.
Definition at line
457
of file
iar.h
.
◆ _BSS_SEGMENT_SIZE
| #define _BSS_SEGMENT_SIZE __segment_size( __BSS__ ) |
Portable segment names.
Definition at line
486
of file
iar.h
.
◆ _CONST_SEGMENT_BEGIN
| #define _CONST_SEGMENT_BEGIN __segment_begin( __CONST__ ) |
Portable segment names.
Definition at line
429
of file
iar.h
.
◆ _CONST_SEGMENT_END
| #define _CONST_SEGMENT_END __segment_end( __CONST__ ) |
Portable segment names.
Definition at line
458
of file
iar.h
.
◆ _CONST_SEGMENT_SIZE
| #define _CONST_SEGMENT_SIZE __segment_size( __CONST__ ) |
Portable segment names.
Definition at line
487
of file
iar.h
.
◆ _CSTACK_SEGMENT_BEGIN
| #define _CSTACK_SEGMENT_BEGIN __segment_begin( __CSTACK__ ) |
Portable segment names.
Definition at line
424
of file
iar.h
.
◆ _CSTACK_SEGMENT_END
| #define _CSTACK_SEGMENT_END __segment_end( __CSTACK__ ) |
Portable segment names.
Definition at line
453
of file
iar.h
.
◆ _CSTACK_SEGMENT_SIZE
| #define _CSTACK_SEGMENT_SIZE __segment_size( __CSTACK__ ) |
Portable segment names.
Definition at line
482
of file
iar.h
.
◆ _DATA_INIT_SEGMENT_BEGIN
| #define _DATA_INIT_SEGMENT_BEGIN __segment_begin( __DATA_INIT__ ) |
Portable segment names.
Definition at line
426
of file
iar.h
.
◆ _DATA_INIT_SEGMENT_END
| #define _DATA_INIT_SEGMENT_END __segment_end( __DATA_INIT__ ) |
Portable segment names.
Definition at line
455
of file
iar.h
.
◆ _DATA_INIT_SEGMENT_SIZE
| #define _DATA_INIT_SEGMENT_SIZE __segment_size( __DATA_INIT__ ) |
Portable segment names.
Definition at line
484
of file
iar.h
.
◆ _DATA_SEGMENT_BEGIN
| #define _DATA_SEGMENT_BEGIN __segment_begin( __DATA__ ) |
Portable segment names.
Definition at line
427
of file
iar.h
.
◆ _DATA_SEGMENT_END
| #define _DATA_SEGMENT_END __segment_end( __DATA__ ) |
Portable segment names.
Definition at line
456
of file
iar.h
.
◆ _DATA_SEGMENT_SIZE
| #define _DATA_SEGMENT_SIZE __segment_size( __DATA__ ) |
Portable segment names.
Definition at line
485
of file
iar.h
.
◆ _DEBUG_CHANNEL_SEGMENT_BEGIN
| #define _DEBUG_CHANNEL_SEGMENT_BEGIN __segment_begin( __DEBUG_CHANNEL__ ) |
Portable segment names.
Definition at line
422
of file
iar.h
.
◆ _DEBUG_CHANNEL_SEGMENT_END
| #define _DEBUG_CHANNEL_SEGMENT_END __segment_end( __DEBUG_CHANNEL__ ) |
Portable segment names.
Definition at line
451
of file
iar.h
.
◆ _DEBUG_CHANNEL_SEGMENT_SIZE
| #define _DEBUG_CHANNEL_SEGMENT_SIZE __segment_size( __DEBUG_CHANNEL__ ) |
Portable segment names.
Definition at line
480
of file
iar.h
.
◆ _DLIB_PERTHREAD_INIT_SEGMENT_BEGIN
| #define _DLIB_PERTHREAD_INIT_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_INIT__ ) |
Portable segment names.
Definition at line
443
of file
iar.h
.
◆ _DLIB_PERTHREAD_INIT_SEGMENT_END
| #define _DLIB_PERTHREAD_INIT_SEGMENT_END __segment_end( __DLIB_PERTHREAD_INIT__ ) |
Portable segment names.
Definition at line
472
of file
iar.h
.
◆ _DLIB_PERTHREAD_INIT_SEGMENT_SIZE
| #define _DLIB_PERTHREAD_INIT_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_INIT__ ) |
Portable segment names.
Definition at line
501
of file
iar.h
.
◆ _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGIN
| #define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_INITIALIZED_DATA__ ) |
Portable segment names.
Definition at line
444
of file
iar.h
.
◆ _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_END
| #define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_END __segment_end( __DLIB_PERTHREAD_INITIALIZED_DATA__ ) |
Portable segment names.
Definition at line
473
of file
iar.h
.
◆ _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZE
| #define _DLIB_PERTHREAD_INITIALIZED_DATA_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_INITIALIZED_DATA__ ) |
Portable segment names.
Definition at line
502
of file
iar.h
.
◆ _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGIN
| #define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_BEGIN __segment_begin( __DLIB_PERTHREAD_ZERO_DATA__ ) |
Portable segment names.
Definition at line
445
of file
iar.h
.
◆ _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_END
| #define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_END __segment_end( __DLIB_PERTHREAD_ZERO_DATA__ ) |
Portable segment names.
Definition at line
474
of file
iar.h
.
◆ _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZE
| #define _DLIB_PERTHREAD_ZERO_DATA_SEGMENT_SIZE __segment_size( __DLIB_PERTHREAD_ZERO_DATA__ ) |
Portable segment names.
Definition at line
503
of file
iar.h
.
◆ _EMHEAP_SEGMENT_BEGIN
| #define _EMHEAP_SEGMENT_BEGIN __segment_begin( __EMHEAP__ ) |
Portable segment names.
Definition at line
441
of file
iar.h
.
◆ _EMHEAP_SEGMENT_END
| #define _EMHEAP_SEGMENT_END __segment_end( __EMHEAP__ ) |
Portable segment names.
Definition at line
470
of file
iar.h
.
◆ _EMHEAP_SEGMENT_SIZE
| #define _EMHEAP_SEGMENT_SIZE __segment_size( __EMHEAP__ ) |
Portable segment names.
Definition at line
499
of file
iar.h
.
◆ _FAT_SEGMENT_BEGIN
| #define _FAT_SEGMENT_BEGIN __segment_begin( __FAT__ ) |
Portable segment names.
Definition at line
436
of file
iar.h
.
◆ _FAT_SEGMENT_END
| #define _FAT_SEGMENT_END __segment_end( __FAT__ ) |
Portable segment names.
Definition at line
465
of file
iar.h
.
◆ _FAT_SEGMENT_SIZE
| #define _FAT_SEGMENT_SIZE __segment_size( __FAT__ ) |
Portable segment names.
Definition at line
494
of file
iar.h
.
◆ _GUARD_REGION_SEGMENT_BEGIN
| #define _GUARD_REGION_SEGMENT_BEGIN __segment_begin( __GUARD_REGION__ ) |
Portable segment names.
Definition at line
442
of file
iar.h
.
◆ _GUARD_REGION_SEGMENT_END
| #define _GUARD_REGION_SEGMENT_END __segment_end( __GUARD_REGION__ ) |
Portable segment names.
Definition at line
471
of file
iar.h
.
◆ _GUARD_REGION_SEGMENT_SIZE
| #define _GUARD_REGION_SEGMENT_SIZE __segment_size( __GUARD_REGION__ ) |
Portable segment names.
Definition at line
500
of file
iar.h
.
◆ _HAL_USE_COMMON_DIVMOD_
| #define _HAL_USE_COMMON_DIVMOD_ |
Use the Divide and Modulus Operations from
platform-common.h
.
Definition at line
307
of file
iar.h
.
◆ _HAL_USE_COMMON_MEMUTILS_
| #define _HAL_USE_COMMON_MEMUTILS_ |
If the line below is uncommented we will use Ember memory APIs, otherwise, we will use the C Standard library (memset,memcpy,memmove) APIs.
Definition at line
520
of file
iar.h
.
◆ _HAL_USE_COMMON_PGM_
| #define _HAL_USE_COMMON_PGM_ |
Use the Master Program Memory Declarations from
platform-common.h
.
Definition at line
126
of file
iar.h
.
◆ _INTERNAL_STORAGE_SEGMENT_BEGIN
| #define _INTERNAL_STORAGE_SEGMENT_BEGIN __segment_begin( __INTERNAL_STORAGE__ ) |
Portable segment names.
Definition at line
446
of file
iar.h
.
◆ _INTERNAL_STORAGE_SEGMENT_END
| #define _INTERNAL_STORAGE_SEGMENT_END __segment_end( __INTERNAL_STORAGE__ ) |
Portable segment names.
Definition at line
475
of file
iar.h
.
◆ _INTERNAL_STORAGE_SEGMENT_SIZE
| #define _INTERNAL_STORAGE_SEGMENT_SIZE __segment_size( __INTERNAL_STORAGE__ ) |
Portable segment names.
Definition at line
504
of file
iar.h
.
◆ _INTVEC_SEGMENT_BEGIN
| #define _INTVEC_SEGMENT_BEGIN __segment_begin( __INTVEC__ ) |
Portable segment names.
Definition at line
423
of file
iar.h
.
◆ _INTVEC_SEGMENT_END
| #define _INTVEC_SEGMENT_END __segment_end( __INTVEC__ ) |
Portable segment names.
Definition at line
452
of file
iar.h
.
◆ _INTVEC_SEGMENT_SIZE
| #define _INTVEC_SEGMENT_SIZE __segment_size( __INTVEC__ ) |
Portable segment names.
Definition at line
481
of file
iar.h
.
◆ _LOCKBITS_IN_MAINFLASH_SEGMENT_BEGIN
| #define _LOCKBITS_IN_MAINFLASH_SEGMENT_BEGIN __segment_begin( __LOCKBITS_IN_MAINFLASH__ ) |
Portable segment names.
Definition at line
447
of file
iar.h
.
◆ _LOCKBITS_IN_MAINFLASH_SEGMENT_END
| #define _LOCKBITS_IN_MAINFLASH_SEGMENT_END __segment_end( __LOCKBITS_IN_MAINFLASH__ ) |
Portable segment names.
Definition at line
476
of file
iar.h
.
◆ _LOCKBITS_IN_MAINFLASH_SEGMENT_SIZE
| #define _LOCKBITS_IN_MAINFLASH_SEGMENT_SIZE __segment_size( __LOCKBITS_IN_MAINFLASH__ ) |
Portable segment names.
Definition at line
505
of file
iar.h
.
◆ _LONGTOKEN_SEGMENT_BEGIN
| #define _LONGTOKEN_SEGMENT_BEGIN __segment_begin( __LONGTOKEN__ ) |
Portable segment names.
Definition at line
440
of file
iar.h
.
◆ _LONGTOKEN_SEGMENT_END
| #define _LONGTOKEN_SEGMENT_END __segment_end( __LONGTOKEN__ ) |
Portable segment names.
Definition at line
469
of file
iar.h
.
◆ _LONGTOKEN_SEGMENT_SIZE
| #define _LONGTOKEN_SEGMENT_SIZE __segment_size( __LONGTOKEN__ ) |
Portable segment names.
Definition at line
498
of file
iar.h
.
◆ _NO_INIT_SEGMENT_BEGIN
| #define _NO_INIT_SEGMENT_BEGIN __segment_begin( __NO_INIT__ ) |
Portable segment names.
Definition at line
421
of file
iar.h
.
◆ _NO_INIT_SEGMENT_END
| #define _NO_INIT_SEGMENT_END __segment_end( __NO_INIT__ ) |
Portable segment names.
Definition at line
450
of file
iar.h
.
◆ _NO_INIT_SEGMENT_SIZE
| #define _NO_INIT_SEGMENT_SIZE __segment_size( __NO_INIT__ ) |
Portable segment names.
Definition at line
479
of file
iar.h
.
◆ _PSSTORE_SEGMENT_BEGIN
| #define _PSSTORE_SEGMENT_BEGIN __segment_begin( __PSSTORE__ ) |
Portable segment names.
Definition at line
439
of file
iar.h
.
◆ _PSSTORE_SEGMENT_END
| #define _PSSTORE_SEGMENT_END __segment_end( __PSSTORE__ ) |
Portable segment names.
Definition at line
468
of file
iar.h
.
◆ _PSSTORE_SEGMENT_SIZE
| #define _PSSTORE_SEGMENT_SIZE __segment_size( __PSSTORE__ ) |
Portable segment names.
Definition at line
497
of file
iar.h
.
◆ _RAT_SEGMENT_BEGIN
| #define _RAT_SEGMENT_BEGIN __segment_begin( __RAT__ ) |
Portable segment names.
Definition at line
437
of file
iar.h
.
◆ _RAT_SEGMENT_END
| #define _RAT_SEGMENT_END __segment_end( __RAT__ ) |
Portable segment names.
Definition at line
466
of file
iar.h
.
◆ _RAT_SEGMENT_SIZE
| #define _RAT_SEGMENT_SIZE __segment_size( __RAT__ ) |
Portable segment names.
Definition at line
495
of file
iar.h
.
◆ _RESETINFO_SEGMENT_BEGIN
| #define _RESETINFO_SEGMENT_BEGIN __segment_begin( __RESETINFO__ ) |
Portable segment names.
Definition at line
425
of file
iar.h
.
◆ _RESETINFO_SEGMENT_END
| #define _RESETINFO_SEGMENT_END __segment_end( __RESETINFO__ ) |
Portable segment names.
Definition at line
454
of file
iar.h
.
◆ _RESETINFO_SEGMENT_SIZE
| #define _RESETINFO_SEGMENT_SIZE __segment_size( __RESETINFO__ ) |
Portable segment names.
Definition at line
483
of file
iar.h
.
◆ _SIMEE_SEGMENT_BEGIN
| #define _SIMEE_SEGMENT_BEGIN __segment_begin( __SIMEE__ ) |
Portable segment names.
Definition at line
438
of file
iar.h
.
◆ _SIMEE_SEGMENT_END
| #define _SIMEE_SEGMENT_END __segment_end( __SIMEE__ ) |
Portable segment names.
Definition at line
467
of file
iar.h
.
◆ _SIMEE_SEGMENT_SIZE
| #define _SIMEE_SEGMENT_SIZE __segment_size( __SIMEE__ ) |
Portable segment names.
Definition at line
496
of file
iar.h
.
◆ _TEXT_SEGMENT_BEGIN
| #define _TEXT_SEGMENT_BEGIN __segment_begin( __TEXT__ ) |
Portable segment names.
Definition at line
430
of file
iar.h
.
◆ _TEXT_SEGMENT_END
| #define _TEXT_SEGMENT_END __segment_end( __TEXT__ ) |
Portable segment names.
Definition at line
459
of file
iar.h
.
◆ _TEXT_SEGMENT_SIZE
| #define _TEXT_SEGMENT_SIZE __segment_size( __TEXT__ ) |
Portable segment names.
Definition at line
488
of file
iar.h
.
◆ _TEXTRW_INIT_SEGMENT_BEGIN
| #define _TEXTRW_INIT_SEGMENT_BEGIN __segment_begin( __TEXTRW_INIT__ ) |
Portable segment names.
Definition at line
431
of file
iar.h
.
◆ _TEXTRW_INIT_SEGMENT_END
| #define _TEXTRW_INIT_SEGMENT_END __segment_end( __TEXTRW_INIT__ ) |
Portable segment names.
Definition at line
460
of file
iar.h
.
◆ _TEXTRW_INIT_SEGMENT_SIZE
| #define _TEXTRW_INIT_SEGMENT_SIZE __segment_size( __TEXTRW_INIT__ ) |
Portable segment names.
Definition at line
489
of file
iar.h
.
◆ _TEXTRW_SEGMENT_BEGIN
| #define _TEXTRW_SEGMENT_BEGIN __segment_begin( __TEXTRW__ ) |
Portable segment names.
Definition at line
432
of file
iar.h
.
◆ _TEXTRW_SEGMENT_END
| #define _TEXTRW_SEGMENT_END __segment_end( __TEXTRW__ ) |
Portable segment names.
Definition at line
461
of file
iar.h
.
◆ _TEXTRW_SEGMENT_SIZE
| #define _TEXTRW_SEGMENT_SIZE __segment_size( __TEXTRW__ ) |
Portable segment names.
Definition at line
490
of file
iar.h
.
◆ _UNRETAINED_RAM_SEGMENT_BEGIN
| #define _UNRETAINED_RAM_SEGMENT_BEGIN __segment_begin( __UNRETAINED_RAM__ ) |
Portable segment names.
Definition at line
448
of file
iar.h
.
◆ _UNRETAINED_RAM_SEGMENT_END
| #define _UNRETAINED_RAM_SEGMENT_END __segment_end( __UNRETAINED_RAM__ ) |
Portable segment names.
Definition at line
477
of file
iar.h
.
◆ _UNRETAINED_RAM_SEGMENT_SIZE
| #define _UNRETAINED_RAM_SEGMENT_SIZE __segment_size( __UNRETAINED_RAM__ ) |
Portable segment names.
Definition at line
506
of file
iar.h
.
◆ ALIGNMENT
| #define ALIGNMENT | ( |
X
|
) | _Pragma( STRINGIZE (data_alignment = X)) |
Provide a portable way to align data.
Definition at line
324
of file
iar.h
.
◆ assert
| #define assert | ( |
condition
|
) |
A custom implementation of the C language assert macro. This macro implements the conditional evaluation and calls the function
halInternalAssertFailed()
. (see
hal/micro/micro.h
)
Definition at line
184
of file
iar.h
.
◆ BIGENDIAN_CPU
| #define BIGENDIAN_CPU false |
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
Definition at line
139
of file
iar.h
.
◆ EEPROM
| #define EEPROM errorerror |
A friendlier name for the compiler's intrinsic for eeprom reference.
Definition at line
158
of file
iar.h
.
◆ HAL_HAS_INT64
| #define HAL_HAS_INT64 |
Denotes that this platform supports 64-bit data-types.
Definition at line
121
of file
iar.h
.
◆ halResetWatchdog
| #define halResetWatchdog | ( |
|
) | halInternalResetWatchDog () |
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
Definition at line
215
of file
iar.h
.
◆ MAIN_FUNCTION_ARGUMENTS
| #define MAIN_FUNCTION_ARGUMENTS |
Definition at line
557
of file
iar.h
.
◆ MAIN_FUNCTION_PARAMETERS
| #define MAIN_FUNCTION_PARAMETERS void |
The kind of arguments the main function takes.
Definition at line
556
of file
iar.h
.
◆ NO_INIT
| #define NO_INIT | ( |
__symbol
|
) | __no_init __symbol |
Provide a portable way to specify a non initialized symbol.
Definition at line
336
of file
iar.h
.
◆ NO_OPERATION
| #define NO_OPERATION | ( |
|
) | __no_operation() |
Define a generic no operation identifier to a compiler specific one.
Definition at line
248
of file
iar.h
.
◆ NO_STRIPPING
| #define NO_STRIPPING __root |
A friendlier name for the compiler's intrinsic for not stripping.
Definition at line
152
of file
iar.h
.
◆ NTOHL
| #define NTOHL | ( |
val
|
) | (__REV(val)) |
A convenient method for code to know what endiannes processor it is running on. For the Cortex-M3, we are little endian.
Definition at line
146
of file
iar.h
.
◆ NTOHS
| #define NTOHS | ( |
val
|
) | (__REV16(val)) |
Define intrinsics for NTOHL and NTOHS to save code space by making endian.c compile to nothing.
Definition at line
145
of file
iar.h
.
◆ PLATCOMMONOKTOINCLUDE
| #define PLATCOMMONOKTOINCLUDE |
Include
platform-common.h
last to pick up defaults and common definitions.
Definition at line
549
of file
iar.h
.
◆ RAMFUNC
| #define RAMFUNC __ramfunc |
Define a generic RAM function identifier to a compiler specific one.
Definition at line
242
of file
iar.h
.
◆ SET_CMSIS_REG
| #define SET_CMSIS_REG | ( |
reg,
|
|
mask,
|
|||
value
|
|||
| ) |
A convenience macro that makes it easy to change a register using the provided mask(s) and value(s). Example: SET_CMSIS_REG(GPIO->P[1].CFGH, (_GPIO_P_CFGH_Px5_MASK | _GPIO_P_CFGH_Px6_MASK), (GPIO_P_CFGH_Px5_OUT | GPIO_P_CFGH_Px6_OUT));.
Definition at line
271
of file
iar.h
.
◆ SET_CMSIS_REG_FIELD
| #define SET_CMSIS_REG_FIELD | ( |
reg,
|
|
field,
|
|||
value
|
|||
| ) |
A convenience macro that makes it easy to change the field of a register, as defined in CMSIS Device headers, to any unsigned value. Example using EM35xx: SET_CMSIS_REG_FIELD(GPIO->P[0].CFGL, GPIO_P_CFGL_Px0, _GPIO_P_CFGL_Px0_OUT);.
Definition at line
282
of file
iar.h
.
◆ SET_REG_FIELD
| #define SET_REG_FIELD | ( |
reg,
|
|
field,
|
|||
value
|
|||
| ) |
A convenience macro that makes it easy to change the field of a register to any unsigned value.
Definition at line
254
of file
iar.h
.
◆ SIGNED_ENUM
| #define SIGNED_ENUM |
Some platforms need to cast enum values that have the high bit set.
Definition at line
227
of file
iar.h
.
◆ simulatedSerialTimePasses
| #define simulatedSerialTimePasses | ( |
|
) |
Stub for code not running in simulation.
Definition at line
302
of file
iar.h
.
◆ simulatedTimePasses
| #define simulatedTimePasses | ( |
|
) |
Stub for code not running in simulation.
Definition at line
292
of file
iar.h
.
◆ simulatedTimePassesMs
| #define simulatedTimePassesMs | ( |
x
|
) |
Stub for code not running in simulation.
Definition at line
297
of file
iar.h
.
◆ STACK_FILL_VALUE
| #define STACK_FILL_VALUE 0xCDCDCDCDU |
Define the magic value that is interpreted by IAR C-SPY's Stack View.
Definition at line
232
of file
iar.h
.
◆ STATIC_ASSERT
| #define STATIC_ASSERT | ( |
__condition,
|
|
__errorstr
|
|||
| ) | static_assert(__condition, __errorstr) |
Provide a portable way to specify a compile time assert.
Definition at line
342
of file
iar.h
.
◆ STRINGIZE
| #define STRINGIZE | ( |
X
|
) | #X |
Convinience macro for turning a token into a string.
Definition at line
319
of file
iar.h
.
◆ UNUSED
| #define UNUSED |
Declare a variable as unused to avoid a warning. Has no effect in IAR builds.
Definition at line
222
of file
iar.h
.
◆ VAR_AT_SEGMENT
| #define VAR_AT_SEGMENT | ( |
__variableDeclaration,
|
|
__segmentName
|
|||
| ) | __variableDeclaration @ __segmentName |
Provide a portable way to specify the segment where a variable lives.
Definition at line
313
of file
iar.h
.
◆ WEAK
| #define WEAK | ( |
__symbol
|
) | __weak __symbol |
Provide a portable way to specify a symbol as weak.
Definition at line
330
of file
iar.h
.
Typedef Documentation
◆ boolean
| typedef bool boolean |
A typedef to make the size of the variable explicitly known.
Definition at line
106
of file
iar.h
.
◆ int16s
| typedef signed short int16s |
A typedef to make the size of the variable explicitly known.
Definition at line
110
of file
iar.h
.
◆ int16u
| typedef unsigned short int16u |
A typedef to make the size of the variable explicitly known.
Definition at line
109
of file
iar.h
.
◆ int32s
| typedef signed int int32s |
A typedef to make the size of the variable explicitly known.
Definition at line
112
of file
iar.h
.
◆ int32u
| typedef unsigned int int32u |
A typedef to make the size of the variable explicitly known.
Definition at line
111
of file
iar.h
.
◆ int64s
| typedef signed long long int64s |
A typedef to make the size of the variable explicitly known.
Definition at line
114
of file
iar.h
.
◆ int64u
| typedef unsigned long long int64u |
A typedef to make the size of the variable explicitly known.
Definition at line
113
of file
iar.h
.
◆ int8s
| typedef signed char int8s |
A typedef to make the size of the variable explicitly known.
Definition at line
108
of file
iar.h
.
◆ int8u
| typedef unsigned char int8u |
A typedef to make the size of the variable explicitly known.
Definition at line
107
of file
iar.h
.
◆ PointerType
| typedef unsigned int PointerType |
A typedef to make the size of the variable explicitly known.
Definition at line
115
of file
iar.h
.
Function Documentation
◆ _executeBarrierInstructions()
| void _executeBarrierInstructions | ( | void |
|
) |
◆ abs()
| int abs | ( | int |
I
|
) |
Returns the absolute value of I (also called the magnitude of I). That is, if I is negative, the result is the opposite of I, but if I is nonnegative the result is I.
- Parameters
-
IAn integer.
- Returns
- A nonnegative integer.
◆ halInternalAssertFailed()
| void halInternalAssertFailed | ( | const char * |
filename,
|
| int |
linenumber
|
||
| ) |
A prototype definition for use by the assert macro. (see
hal/micro/micro.h
)
◆ halInternalResetWatchDog()
| void halInternalResetWatchDog | ( | void |
|
) |
Macro to reset the watchdog timer. Note: be very very careful when using this as you can easily get into an infinite loop if you are not careful.