WSTK Sensors Plugin
Set of APIs for WSTK sensors plugin. More...
Functions |
|
| EmberStatus | emberAfPluginWstkSensorsGetSample (uint32_t *rhData, int32_t *tData) |
|
Read a sample of the temperature and relative humidity values from the WSTK Si7013 sensors.
More...
|
|
Detailed Description
Set of APIs for WSTK sensors plugin.
See
wstk-sensors.h
for source code.
Function Documentation
◆ emberAfPluginWstkSensorsGetSample()
| EmberStatus emberAfPluginWstkSensorsGetSample | ( | uint32_t * |
rhData,
|
| int32_t * |
tData
|
||
| ) |
Read a sample of the temperature and relative humidity values from the WSTK Si7013 sensors.
- Parameters
-
rhDataA pointer to a 32-bit unsigned integer where the relative humidity sample is written. tDataA pointer to a 32-bit signed integer where the temperature is written. Temperature is sampled in "millicelsius".
- Returns
-
An
EmberStatusvalue of EMBER_SUCCESS if the relative humidity and temperature sample were successfully read from the Si7013 sensors. Otherwise, anEmberStatusvalue of EMBER_ERR_FATAL .