EmberNetworkParameters Struct Reference
Hold network parameters. More...
#include <
ember-types.h
>
Data Fields |
|
| uint16_t | panId |
| int8_t | radioTxPower |
| uint8_t | radioChannel |
Hold network parameters.
For information about power settings and radio channels, see the technical specification for the RF communication module in your Developer Kit and the Radio Configurator Guide (AN971).
Definition at line
163
of file
ember-types.h
.
Field Documentation
◆ panId
| uint16_t EmberNetworkParameters::panId |
The network's PAN identifier.
Definition at line
165
of file
ember-types.h
.
◆ radioChannel
| uint8_t EmberNetworkParameters::radioChannel |
The radio channel. Be sure to specify a channel supported by the radio.
Definition at line
169
of file
ember-types.h
.
◆ radioTxPower
| int8_t EmberNetworkParameters::radioTxPower |
The transmit power setting, in dBm.
Definition at line
167
of file
ember-types.h
.
The documentation for this struct was generated from the following file:
-
ember-types.h