EmberIncomingMacMessage Struct Reference
An instance of this structure is passed to emberIncomingMacMessageHandler() . It describes the incoming MAC frame. More...
#include <
ember-types.h
>
Data Fields |
|
| EmberMessageOptions | options |
| EmberMacFrame | macFrame |
| int8_t | rssi |
| int8_t | lqi |
| uint32_t | frameCounter |
| EmberMessageLength | length |
| uint8_t * | payload |
An instance of this structure is passed to emberIncomingMacMessageHandler() . It describes the incoming MAC frame.
Definition at line
374
of file
ember-types.h
.
Field Documentation
◆ frameCounter
| uint32_t EmberIncomingMacMessage::frameCounter |
The security MAC frame counter (if any).
Definition at line
396
of file
ember-types.h
.
◆ length
| EmberMessageLength EmberIncomingMacMessage::length |
An EmberMessageLength value indicating the length in bytes of the MAC payload of the incoming message.
Definition at line
401
of file
ember-types.h
.
◆ lqi
| int8_t EmberIncomingMacMessage::lqi |
The LQI the packet was received with.
Definition at line
392
of file
ember-types.h
.
◆ macFrame
| EmberMacFrame EmberIncomingMacMessage::macFrame |
An EmberMacFrame structure indicating the source and destination addresses and source and destination PAN IDs.
Definition at line
384
of file
ember-types.h
.
◆ options
| EmberMessageOptions EmberIncomingMacMessage::options |
An EmberMessageOptions value indicating the options used for the incoming packet.
Definition at line
379
of file
ember-types.h
.
◆ payload
| uint8_t* EmberIncomingMacMessage::payload |
A pointer to the message MAC payload.
Definition at line
405
of file
ember-types.h
.
◆ rssi
| int8_t EmberIncomingMacMessage::rssi |
The RSSI in dBm the packet was received with.
Definition at line
388
of file
ember-types.h
.
The documentation for this struct was generated from the following file:
-
ember-types.h