EmberOutgoingMessage Struct Reference
An instance of this structure is passed to emberMessageSentHandler(). It describes the outgoing packet. More...
#include <
ember-types.h
>
Data Fields | |
EmberMessageOptions | options |
EmberNodeId | destination |
uint8_t | endpoint |
uint8_t | tag |
EmberMessageLength | length |
uint8_t * | payload |
int8_t | ackRssi |
An instance of this structure is passed to emberMessageSentHandler(). It describes the outgoing packet.
Definition at line 262
of file ember-types.h
.
Field Documentation
◆ ackRssi
int8_t EmberOutgoingMessage::ackRssi |
The RSSI in dBm of the ACK corresponding to this message. This field is meaningful only if EMBER_OPTIONS_ACK_REQUESTED flag is set in the options field.
Definition at line 295
of file ember-types.h
.
◆ destination
EmberNodeId EmberOutgoingMessage::destination |
An EmberNodeId value indicating the destination short ID.
Definition at line 271
of file ember-types.h
.
◆ endpoint
uint8_t EmberOutgoingMessage::endpoint |
The endpoint the message is destined to.
Definition at line 275
of file ember-types.h
.
◆ length
EmberMessageLength EmberOutgoingMessage::length |
An EmberMessageLength value indicating the length in bytes of the incoming message.
Definition at line 285
of file ember-types.h
.
◆ options
EmberMessageOptions EmberOutgoingMessage::options |
An EmberMessageOptions value indicating the options used for transmitting the outgoing message.
Definition at line 267
of file ember-types.h
.
◆ payload
uint8_t* EmberOutgoingMessage::payload |
A pointer to the message payload.
Definition at line 289
of file ember-types.h
.
◆ tag
uint8_t EmberOutgoingMessage::tag |
A tag value the application can use to match emberMessageSend() calls to the corresponding emberMessageSentHandler() calls.
Definition at line 280
of file ember-types.h
.
The documentation for this struct was generated from the following file:
ember-types.h