EmberMacAddress Struct Reference
A structure that stores an 802.15.4 address. More...
#include <
ember-types.h
>
Data Fields | |
union { | |
uint8_t longAddress [EUI64_SIZE] | |
Long (EUI-64) address. Valid if mode is EMBER_MAC_ADDRESS_MODE_LONG. More... | |
uint16_t shortAddress | |
Short address (node ID). Valid if mode is EMBER_MAC_ADDRESS_MODE_SHORT. More... | |
} | addr |
EmberMacAddressMode | mode |
A structure that stores an 802.15.4 address.
Definition at line 319
of file ember-types.h
.
Field Documentation
◆ addr
union { ... } EmberMacAddress::addr |
◆ longAddress
uint8_t EmberMacAddress::longAddress[EUI64_SIZE] |
Long (EUI-64) address. Valid if mode
is EMBER_MAC_ADDRESS_MODE_LONG.
Definition at line 325
of file ember-types.h
.
◆ mode
EmberMacAddressMode EmberMacAddress::mode |
Addressing mode
Definition at line 333
of file ember-types.h
.
◆ shortAddress
uint16_t EmberMacAddress::shortAddress |
Short address (node ID). Valid if mode
is EMBER_MAC_ADDRESS_MODE_SHORT.
Definition at line 330
of file ember-types.h
.
The documentation for this struct was generated from the following file:
ember-types.h